Prezentare generală a produsului
UK003010 is a PICSTART Plus Flash, reprogrammable firmware upgrade. This PICSTART Plus Flash Upgrade Module (PUM) is a PCB that contains a PIC18F6720 device that has been programmed with the firmware needed to provide support for a specific set of devices in the MPLAB IDE. The PUM is used to replace the PIC17C44 inside of the PICSTART Plus, the device that contains the firmware that can provide support to a maximum firmware version 3.11 in the MPLAB IDE. Because the PUM uses Flash technology, its firmware can be upgraded as needed to gain support for new devices by using an option in the MPLAB IDE.
- C compiler friendly development environment
- 1024 bytes of EEPROM
- An in-circuit debugger
- Self programming
- Synchronous serial port configured as either 3 wire SPI or 2 wire I2C bus
- Two addressable universal asynchronous receiver transmitter
Aplicaţii
Communications & Networking, Sensing & Instrumentation, System Monitoring, Consumer Electronics, Audio
Note
90 Day Warranty only. After Expiration of Warranty returns must be processed via Microchip.
Specificaţii tehnice
PIC18F
Adds support for a specific set of devices in the MPLAB® IDE, flash based,
PUM unit
-
Documentaţie tehnică (2)
Produse asociate
3 produse găsite
Legislaţie şi reglementări privind protecţia mediului
Tara in care ultimul proces semnificativ de fabricare a fost efectuatŢara de origine:United States
Tara in care ultimul proces semnificativ de fabricare a fost efectuat
Certificat de conformitate produs